The display is limited in the number of digits that it can display because of the physical size of the display. If the readback value is read from the interface then it will pass as many digits as it has available to give full accuracy of the readback value.
Applies to: AC6801A, AC6802A, AC6803A, AC6804A
Applies to: 6811B, 6812B, 6813B
Visit our Power Products Forum for additional topics and discussions. Read technical postings on our Power Blog – Watt’s Up? |